About i.MX RT1020 SDK ram_allocate sample

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About i.MX RT1020 SDK ram_allocate sample

Jump to solution
1,172 Views
ogawatakeshi
Contributor II

Flexram.PNG

pastedImage_2.png

I tried ram allocation sample.

as a result, I think that ITCM and DTCM are opposite.
Is this wrong?

best regards

Labels (1)
1 Solution
1,000 Views
igorpadykov
NXP Employee
NXP Employee

Hi OGAWA

based on provided parts of code I believe you are right that ITCM and DTCM are opposite.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
1,001 Views
igorpadykov
NXP Employee
NXP Employee

Hi OGAWA

based on provided parts of code I believe you are right that ITCM and DTCM are opposite.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,000 Views
ogawatakeshi
Contributor II

Thanks igor.

I hope it will be fixed in the next SDK update.

Bst rgd!

0 Kudos