we do not have any particular example as the process is quite simple:
To control error injection configure Memory Error Control Register (CAN_MECR) and set address for error injection:
The error injection is done via Error Injection Address Register (CAN_ERRIAR)
40.4.21 Error Injection Address Register (CAN_ERRIAR) This register holds the address where error is to be injected. Use the following table to convert from the memory map address to the location in the physical FlexCAN RAM.
Hi,
we do not have any particular example as the process is quite simple:
To control error injection configure Memory Error Control Register (CAN_MECR) and set address for error injection:
The error injection is done via Error Injection Address Register (CAN_ERRIAR)
40.4.21 Error Injection Address Register (CAN_ERRIAR)
This register holds the address where error is to be injected. Use the following table to convert from the memory map address to the location in the physical FlexCAN RAM.
regards,
Peter