IMX6D Pop LDDR2 questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D Pop LDDR2 questions

Jump to solution
627 Views
lane
Contributor I

We would like to use the IMX6D pop package but cannot find documentation on what LPDDR2 dram's are supported. I found in another post that the micron MT42L128M64D2LL-25 AT is supported, but that part is now obsolete. Micron lists EDB8164B4PT-1DIT-F as a replacement, but I don't know if it is supported. Are there other manufacturers we can consider as well?

The POP package does not seem very popular, which I don't understand. It seems like a great solution to save space and board complexity. What are the negatives? Am I wrong in my perception that it is not very popular?

Labels (2)
0 Kudos
1 Solution
499 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lane

for other supported memories one can look at

Table 1. Validated memory parts AN11937 SCM-i.MX6DQ PoP Memory Application Note
https://www.nxp.com/docs/en/application-note/AN11937.pdf

Other useful documentation is available on link

Single Chip Module-i.MX 6D|NXP 

Best regards
igor
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
500 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lane

for other supported memories one can look at

Table 1. Validated memory parts AN11937 SCM-i.MX6DQ PoP Memory Application Note
https://www.nxp.com/docs/en/application-note/AN11937.pdf

Other useful documentation is available on link

Single Chip Module-i.MX 6D|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos