About "Imx 8MD" chip ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About "Imx 8MD" chip ?

409 Views
传策薛
Contributor V

Hi community:

     Where is the "Imx 8MD" Android BSP,?  Is same as the Android8.1?

0 Kudos
1 Reply

331 Views
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛 

yes it is the same, number of cores can be set with kernel boot parameter maxcpus=n

as described in linux/Documentation/kernel-parameters.txt

kernel-parameters.txt\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos