AnsweredAssumed Answered

MCUXpresso with LPC-LINK2 having error "Target error from Commit Flash write"

Question asked by Jason Lu on Oct 24, 2018
Latest reply on Oct 29, 2018 by Victor Jimenez

Hi,

I am using MCUXpresso IDE with LPC-LINK2 on a board with LPC1769 processor.

The same board and the same code I can use LPCXpresso IDE with LPC-LINK1 or LPC-LINK2 as debugger.

I can use MCUXpresso IDE with LPC-LINK1 as debugger.

However, when I try to use MCUXpresso IDE with LPC-LINK2 as debugger, I will receive the following error:

 

failed to send op Terminate message - rc Em(17). Debug port inaccessible after access at location 0x10002620
Target error from Commit Flash write: Em(17). Debug port inaccessible after access at location 0x10002620

 

The board is powered through its own power supply, and as the LPC-LINK2 can work with LPCXpresso IDE, I don't think it is a hardware problem.

 

Any thoughts, suggestions?

 

Thanks!

Outcomes