AnsweredAssumed Answered

I’m trying to interface SLIC IC 32287 with iMX6q processor.

Question asked by Snehal Jadhav on Oct 23, 2018
Latest reply on Nov 19, 2019 by Abhijeet Gokar

The SI32287 provides SPI and PCM interface to host. Also, the SPI interface pins SCLK, SPI_MOSI, SPI_MISO, & CHIP SELECT are mapped to Processors SPI port and the PCM interface pins MOSI, MISO, PCLK and frame Sync are mapped to the processor AudioMux port5(act as PCM).

 

The minimum PCLK frequency for PCM interface of SLIC IC should be 512KHz according to the datasheet. PCLK signal is mapped to TXC pin of AUDMUX Port 5 of processor.

Will the processor be able to generate 512KHz of frequency at TXC pin?

 

Also, the PCLK frequency is dependent on the frame sync. My frame sync frequency is fixed of 8KHz.

 

 

Is the configuration possible for frame sync of 8KHz, Word-length of 64bits(for dual channel of SLIC) and PCLK of 512KHz?

Outcomes