AnsweredAssumed Answered

SDK builder for IAR?

Question asked by Nick Dolling on Oct 22, 2018
Latest reply on Oct 23, 2018 by Nick Dolling

Hi,

I'm evaluating the K27 and the iMX-RT1064 for a new project. We plan to use IAR, and as I'm not familiar with MCUXpresso, I hoped to use the example projects to allow me to evaluate a few things on each quickly.

 

When I generate the SDK for the MIMXRT1060EVK.. it asks me which toolchain I want, but when I do it for the FRDM-K28F, it doesn't give me the option and just generates if for MCUXpresso, and there are no IAR workspaces set up for the example projects.

 

The doco for the SDK (which seems a bit old) says that there should be example project files for all the various supported toolchains... where have they gone?

 

Thanks,

 

Nick

Outcomes