AnsweredAssumed Answered

Installation Sensory TrulyHandsfree SDK and license i.MX8M

Question asked by Cesar Hernandez on Oct 22, 2018
Latest reply on Oct 23, 2018 by Cesar Hernandez

Hi All,

 

I have build Alexa SDK (AVS) and  installed the image for i.MX8M evk board (with Yocto Morty, Kernel 4.9) based on this document: Build Alexa SDK (AVS) image for i.MX8M EVK board (with Yocto Morty, Kernel4.9) 

 

The issue I am having is installing the SDK and license for the Sensory TrulyHandsfree on this image. In the section of the document to Install Alexa SDK it reads this message:

If you select YES, then your image will contain the AVS SDK ready to use (after authentication). Note this AVS_SDK will not have WakeWord detection support, but it can be added on runtime.

If your selection was NO, then you can always manually fetch and build the AVS_SDK on runtime. All the packages dependencies will be already there, so only fetching the AVS_SDK source code and building it is required.

I have the Sensory TrulyHandsfree SDK ready on hand and license ready to license but have no idea how to add WakeWord detection on runtime.

My question is if someone has any idea on how to install the Sensory TrulyHandsfree SDK and license on runtime so WakeWord detection will work for this image. Any help is appreciated.

Thank You.

Outcomes