How can I use the SDK realise next function:
the MCU is the master device, I want to use flexio or LPI2C read/write slave device subaddress(such as EEPROM , own subaddress). I lookup the SDK interface, dont get the subaddress access operation.
How CAN I do it use the SDK?
Hi,
You need to use the SDK functions, such as LPI2C_DRV_MasterSendDataBlocking(), to send a sub-address or a command to the slave, you also need to specify if the function will send Stop condition - the function takes that as an argument. The SDK PE interface allows you to select the address of the slave device only.
Regards,
Daniel