Hello,
I found that neither the SDK provided by NXP nor the examples provided by Keil show how to initialize the SD card on the IMXRT1050 board (mine is the 1052DVL68). I know that the SDK comes with fatfs middleware, but the middleware examples didn't include one for the SD card. Some of the Keil examples use the CORE file system component, but that requires a Keil MDK Plus license, and I only have the essential license. I do have the fsl_usdhc.c driver.
Has anyone set up the SD peripheral correctly under these conditions?
For reference, here's what I've tried so far
I've used the clock_config and pin_mux code, provided by the MassStorage example (downloaded using the Keil pack installer). I will post those last because they are so long. After setting up the pin muxing and clock configuration, I used the following setup code:
usdhc_config_t sd_config;
usdhc_handle_t handle;
usdhc_transfer_callback_t transfer_callback;
sd_config.dataTimeout = 0xFU; /*!< Data timeout value */
sd_config.endianMode = kUSDHC_EndianModeLittle; /*!< Endian mode */
sd_config.readWatermarkLevel = 128; /*!< Watermark level for DMA read operation. Available range is 1 ~ 128. (words)*/
sd_config.writeWatermarkLevel = 128; /*!< Watermark level for DMA write operation. Available range is 1 ~ 128. (words) */
sd_config.readBurstLen = 16; /*!< Read burst len (words)*/
sd_config.writeBurstLen = 16; /*!< Write burst len (words) */
/* Configure the uSD device */
USDHC_Init(SD_DRIVER, &sd_config);
transfer_callback.CardInserted = CardInserted;
transfer_callback.CardRemoved = CardRemoved;
transfer_callback.SdioInterrupt = SdioInterrupt;
transfer_callback.BlockGap = BlockGap;
transfer_callback.TransferComplete = TransferComplete;
transfer_callback.ReTuning = ReTuning;
USDHC_TransferCreateHandle(SD_DRIVER, &handle, &transfer_callback, NULL);
USDHC_SetSdClock(SD_DRIVER, SystemCoreClock, 48 * (2 << 20));
USDHC_SetDataBusWidth (SD_DRIVER, kUSDHC_DataBusWidth4Bit);
if (USDHC_SetCardActive(SD_DRIVER, 48 * (2 << 20)) == false)
{
printf("failed to set sd card active\r\n");
return STA_NOINIT;
}
SD_DRIVER->INT_SIGNAL_EN = (
USDHC_INT_SIGNAL_EN_DTOEIEN(1) | USDHC_INT_SIGNAL_EN_CIEIEN(1) | USDHC_INT_SIGNAL_EN_CTOEIEN(1) | USDHC_INT_SIGNAL_EN_CINTIEN(1) | USDHC_INT_SIGNAL_EN_CRMIEN(1)
| USDHC_INT_SIGNAL_EN_CINSIEN(1) |USDHC_INT_SIGNAL_EN_TCIEN(1) | USDHC_INT_SIGNAL_EN_CCIEN(1)
);
if ((SD_DRIVER->PRES_STATE & USDHC_PRES_STATE_CINST_MASK) == 0)
return STA_NODISK;
I get to this point and return STA_NODISK, when a card is inserted. It appears the peripheral isn't enabled. However, I set up the pins as follows:
CLOCK_EnableClock(kCLOCK_Iomuxc); /* iomuxc clock (iomuxc_clk_enable): 0x03u */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_12_GPIO2_IO28, /* GPIO_B1_12 is configured as GPIO2_IO28 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_00_USDHC1_CMD, /* GPIO_SD_B0_00 is configured as USDHC1_CMD */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_01_USDHC1_CLK, /* GPIO_SD_B0_01 is configured as USDHC1_CLK */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_02_USDHC1_DATA0, /* GPIO_SD_B0_02 is configured as USDHC1_DATA0 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_03_USDHC1_DATA1, /* GPIO_SD_B0_03 is configured as USDHC1_DATA1 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_04_USDHC1_DATA2, /* GPIO_SD_B0_04 is configured as USDHC1_DATA2 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_05_USDHC1_DATA3, /* GPIO_SD_B0_05 is configured as USDHC1_DATA3 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_00_USDHC1_CMD, /* GPIO_SD_B0_00 PAD functional properties : */
0x70C9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Pull
Pull Up / Down Config. Field: 47K Ohm Pull Up
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_01_USDHC1_CLK, /* GPIO_SD_B0_01 PAD functional properties : */
0xC9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Disabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_02_USDHC1_DATA0, /* GPIO_SD_B0_02 PAD functional properties : */
0x70C9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Pull
Pull Up / Down Config. Field: 47K Ohm Pull Up
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_03_USDHC1_DATA1, /* GPIO_SD_B0_03 PAD functional properties : */
0x70C9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Pull
Pull Up / Down Config. Field: 47K Ohm Pull Up
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_04_USDHC1_DATA2, /* GPIO_SD_B0_04 PAD functional properties : */
0x70C9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Pull
Pull Up / Down Config. Field: 47K Ohm Pull Up
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_SD_B0_05_USDHC1_DATA3, /* GPIO_SD_B0_05 PAD functional properties : */
0x70C9u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0(150 Ohm @ 3.3V, 260 Ohm@1.8V)
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Pull
Pull Up / Down Config. Field: 47K Ohm Pull Up
Hyst. Enable Field: Hysteresis Disabled */
and I set up the clock as follows:
/* Init RTC OSC clock frequency. */
CLOCK_SetRtcXtalFreq(32768U);
/* Enable 1MHz clock output. */
XTALOSC24M->OSC_CONFIG2 |= XTALOSC24M_OSC_CONFIG2_ENABLE_1M_MASK;
/* Use free 1MHz clock output. */
XTALOSC24M->OSC_CONFIG2 &= ~XTALOSC24M_OSC_CONFIG2_MUX_1M_MASK;
/* Set XTAL 24MHz clock frequency. */
CLOCK_SetXtalFreq(24000000U);
/* Enable XTAL 24MHz clock source. */
CLOCK_InitExternalClk(0);
/* Enable internal RC. */
CLOCK_InitRcOsc24M();
/* Switch clock source to external OSC. */
CLOCK_SwitchOsc(kCLOCK_XtalOsc);
/* Set Oscillator ready counter value. */
CCM->CCR = (CCM->CCR & (~CCM_CCR_OSCNT_MASK)) | CCM_CCR_OSCNT(127);
/* Setting PeriphClk2Mux and PeriphMux to provide stable clock before PLLs are initialed */
CLOCK_SetMux(kCLOCK_PeriphClk2Mux, 1); /* Set PERIPH_CLK2 MUX to OSC */
CLOCK_SetMux(kCLOCK_PeriphMux, 1); /* Set PERIPH_CLK MUX to PERIPH_CLK2 */
/* Setting the VDD_SOC to 1.5V. It is necessary to config AHB to 600Mhz. */
DCDC->REG3 = (DCDC->REG3 & (~DCDC_REG3_TRG_MASK)) | DCDC_REG3_TRG(0x12);
/* Waiting for DCDC_STS_DC_OK bit is asserted */
while (DCDC_REG0_STS_DC_OK_MASK != (DCDC_REG0_STS_DC_OK_MASK & DCDC->REG0))
{
}
/* Init ARM PLL. */
CLOCK_InitArmPll(&armPllConfig_BOARD_BootClockRUN);
/* In SDK projects, SDRAM (configured by SEMC) will be initialized in either debug script or dcd.
* With this macro SKIP_SYSCLK_INIT, system pll (selected to be SEMC source clock in SDK projects) will be left unchanged.
* Note: If another clock source is selected for SEMC, user may want to avoid changing that clock as well.*/
#ifndef SKIP_SYSCLK_INIT
/* Init System PLL. */
CLOCK_InitSysPll(&sysPllConfig_BOARD_BootClockRUN);
/* Init System pfd0. */
CLOCK_InitSysPfd(kCLOCK_Pfd0, 27);
/* Init System pfd1. */
CLOCK_InitSysPfd(kCLOCK_Pfd1, 16);
/* Init System pfd2. */
CLOCK_InitSysPfd(kCLOCK_Pfd2, 24);
/* Init System pfd3. */
CLOCK_InitSysPfd(kCLOCK_Pfd3, 16);
/* Disable pfd offset. */
CCM_ANALOG->PLL_SYS &= ~CCM_ANALOG_PLL_SYS_PFD_OFFSET_EN_MASK;
#endif
/* In SDK projects, external flash (configured by FLEXSPI) will be initialized by dcd.
* With this macro XIP_EXTERNAL_FLASH, usb1 pll (selected to be FLEXSPI clock source in SDK projects) will be left unchanged.
* Note: If another clock source is selected for FLEXSPI, user may want to avoid changing that clock as well.*/
#if !(defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1))
/* Init Usb1 PLL. */
CLOCK_InitUsb1Pll(&usb1PllConfig_BOARD_BootClockRUN);
/* Init Usb1 pfd0. */
CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 33);
/* Init Usb1 pfd1. */
CLOCK_InitUsb1Pfd(kCLOCK_Pfd1, 16);
/* Init Usb1 pfd2. */
CLOCK_InitUsb1Pfd(kCLOCK_Pfd2, 17);
/* Init Usb1 pfd3. */
CLOCK_InitUsb1Pfd(kCLOCK_Pfd3, 19);
/* Disable Usb1 PLL output for USBPHY1. */
CCM_ANALOG->PLL_USB1 &= ~CCM_ANALOG_PLL_USB1_EN_USB_CLKS_MASK;
#endif
/* DeInit Audio PLL. */
CLOCK_DeinitAudioPll();
/* Bypass Audio PLL. */
CLOCK_SetPllBypass(CCM_ANALOG, kCLOCK_PllAudio, 1);
/* Set divider for Audio PLL. */
CCM_ANALOG->MISC2 &= ~CCM_ANALOG_MISC2_AUDIO_DIV_LSB_MASK;
CCM_ANALOG->MISC2 &= ~CCM_ANALOG_MISC2_AUDIO_DIV_MSB_MASK;
/* Enable Audio PLL output. */
CCM_ANALOG->PLL_AUDIO |= CCM_ANALOG_PLL_AUDIO_ENABLE_MASK;
/* DeInit Video PLL. */
CLOCK_DeinitVideoPll();
/* Bypass Video PLL. */
CCM_ANALOG->PLL_VIDEO |= CCM_ANALOG_PLL_VIDEO_BYPASS_MASK;
/* Set divider for Video PLL. */
CCM_ANALOG->MISC2 = (CCM_ANALOG->MISC2 & (~CCM_ANALOG_MISC2_VIDEO_DIV_MASK)) | CCM_ANALOG_MISC2_VIDEO_DIV(0);
/* Enable Video PLL output. */
CCM_ANALOG->PLL_VIDEO |= CCM_ANALOG_PLL_VIDEO_ENABLE_MASK;
/* DeInit Enet PLL. */
CLOCK_DeinitEnetPll();
/* Bypass Enet PLL. */
CLOCK_SetPllBypass(CCM_ANALOG, kCLOCK_PllEnet, 1);
/* Set Enet output divider. */
CCM_ANALOG->PLL_ENET = (CCM_ANALOG->PLL_ENET & (~CCM_ANALOG_PLL_ENET_DIV_SELECT_MASK)) | CCM_ANALOG_PLL_ENET_DIV_SELECT(1);
/* Enable Enet output. */
CCM_ANALOG->PLL_ENET |= CCM_ANALOG_PLL_ENET_ENABLE_MASK;
/* Enable Enet25M output. */
CCM_ANALOG->PLL_ENET |= CCM_ANALOG_PLL_ENET_ENET_25M_REF_EN_MASK;
/* DeInit Usb2 PLL. */
CLOCK_DeinitUsb2Pll();
/* Bypass Usb2 PLL. */
CLOCK_SetPllBypass(CCM_ANALOG, kCLOCK_PllUsb2, 1);
/* Enable Usb2 PLL output. */
CCM_ANALOG->PLL_USB2 |= CCM_ANALOG_PLL_USB2_ENABLE_MASK;
/* Set AHB_PODF. */
CLOCK_SetDiv(kCLOCK_AhbDiv, 0);
/* Set IPG_PODF. */
CLOCK_SetDiv(kCLOCK_IpgDiv, 3);
/* Set ARM_PODF. */
CLOCK_SetDiv(kCLOCK_ArmDiv, 1);
/* Set preperiph clock source. */
CLOCK_SetMux(kCLOCK_PrePeriphMux, 3);
/* Set periph clock source. */
CLOCK_SetMux(kCLOCK_PeriphMux, 0);
/* Set PERIPH_CLK2_PODF. */
CLOCK_SetDiv(kCLOCK_PeriphClk2Div, 0);
/* Set periph clock2 clock source. */
CLOCK_SetMux(kCLOCK_PeriphClk2Mux, 0);
/* Set PERCLK_PODF. */
CLOCK_SetDiv(kCLOCK_PerclkDiv, 1);
/* Set per clock source. */
CLOCK_SetMux(kCLOCK_PerclkMux, 0);
/* Set USDHC1_PODF. */
CLOCK_SetDiv(kCLOCK_Usdhc1Div, 1);
/* Set Usdhc1 clock source. */
CLOCK_SetMux(kCLOCK_Usdhc1Mux, 0);
/* Set USDHC2_PODF. */
CLOCK_SetDiv(kCLOCK_Usdhc2Div, 1);
/* Set Usdhc2 clock source. */
CLOCK_SetMux(kCLOCK_Usdhc2Mux, 0);
/* In SDK projects, SDRAM (configured by SEMC) will be initialized in either debug script or dcd.
* With this macro SKIP_SYSCLK_INIT, system pll (selected to be SEMC source clock in SDK projects) will be left unchanged.
* Note: If another clock source is selected for SEMC, user may want to avoid changing that clock as well.*/
#ifndef SKIP_SYSCLK_INIT
/* Set SEMC_PODF. */
CLOCK_SetDiv(kCLOCK_SemcDiv, 7);
/* Set Semc alt clock source. */
CLOCK_SetMux(kCLOCK_SemcAltMux, 0);
/* Set Semc clock source. */
CLOCK_SetMux(kCLOCK_SemcMux, 0);
#endif
/* In SDK projects, external flash (configured by FLEXSPI) will be initialized by dcd.
* With this macro XIP_EXTERNAL_FLASH, usb1 pll (selected to be FLEXSPI clock source in SDK projects) will be left unchanged.
* Note: If another clock source is selected for FLEXSPI, user may want to avoid changing that clock as well.*/
#if !(defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1))
/* Set FLEXSPI_PODF. */
CLOCK_SetDiv(kCLOCK_FlexspiDiv, 0);
/* Set Flexspi clock source. */
CLOCK_SetMux(kCLOCK_FlexspiMux, 3);
#endif
/* Set CSI_PODF. */
CLOCK_SetDiv(kCLOCK_CsiDiv, 1);
/* Set Csi clock source. */
CLOCK_SetMux(kCLOCK_CsiMux, 0);
/* Set LPSPI_PODF. */
CLOCK_SetDiv(kCLOCK_LpspiDiv, 4);
/* Set Lpspi clock source. */
CLOCK_SetMux(kCLOCK_LpspiMux, 2);
/* Set TRACE_PODF. */
CLOCK_SetDiv(kCLOCK_TraceDiv, 2);
/* Set Trace clock source. */
CLOCK_SetMux(kCLOCK_TraceMux, 2);
/* Set SAI1_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Sai1PreDiv, 3);
/* Set SAI1_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Sai1Div, 1);
/* Set Sai1 clock source. */
CLOCK_SetMux(kCLOCK_Sai1Mux, 0);
/* Set SAI2_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Sai2PreDiv, 3);
/* Set SAI2_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Sai2Div, 1);
/* Set Sai2 clock source. */
CLOCK_SetMux(kCLOCK_Sai2Mux, 0);
/* Set SAI3_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Sai3PreDiv, 3);
/* Set SAI3_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Sai3Div, 1);
/* Set Sai3 clock source. */
CLOCK_SetMux(kCLOCK_Sai3Mux, 0);
/* Set LPI2C_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Lpi2cDiv, 0);
/* Set Lpi2c clock source. */
CLOCK_SetMux(kCLOCK_Lpi2cMux, 0);
/* Set CAN_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_CanDiv, 1);
/* Set Can clock source. */
CLOCK_SetMux(kCLOCK_CanMux, 2);
/* Set UART_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_UartDiv, 0);
/* Set Uart clock source. */
CLOCK_SetMux(kCLOCK_UartMux, 0);
/* Set LCDIF_PRED. */
CLOCK_SetDiv(kCLOCK_LcdifPreDiv, 1);
/* Set LCDIF_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_LcdifDiv, 3);
/* Set Lcdif pre clock source. */
CLOCK_SetMux(kCLOCK_LcdifPreMux, 5);
/* Set SPDIF0_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Spdif0PreDiv, 1);
/* Set SPDIF0_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Spdif0Div, 7);
/* Set Spdif clock source. */
CLOCK_SetMux(kCLOCK_SpdifMux, 3);
/* Set FLEXIO1_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Flexio1PreDiv, 1);
/* Set FLEXIO1_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Flexio1Div, 7);
/* Set Flexio1 clock source. */
CLOCK_SetMux(kCLOCK_Flexio1Mux, 3);
/* Set FLEXIO2_CLK_PRED. */
CLOCK_SetDiv(kCLOCK_Flexio2PreDiv, 1);
/* Set FLEXIO2_CLK_PODF. */
CLOCK_SetDiv(kCLOCK_Flexio2Div, 7);
/* Set Flexio2 clock source. */
CLOCK_SetMux(kCLOCK_Flexio2Mux, 3);
/* Set Pll3 sw clock source. */
CLOCK_SetMux(kCLOCK_Pll3SwMux, 0);
/* Set lvds1 clock source. */
CCM_ANALOG->MISC1 = (CCM_ANALOG->MISC1 & (~CCM_ANALOG_MISC1_LVDS1_CLK_SEL_MASK)) | CCM_ANALOG_MISC1_LVDS1_CLK_SEL(0);
/* Set clock out1 divider. */
CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_DIV_MASK)) | CCM_CCOSR_CLKO1_DIV(0);
/* Set clock out1 source. */
CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_SEL_MASK)) | CCM_CCOSR_CLKO1_SEL(1);
/* Set clock out2 divider. */
CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO2_DIV_MASK)) | CCM_CCOSR_CLKO2_DIV(0);
/* Set clock out2 source. */
CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO2_SEL_MASK)) | CCM_CCOSR_CLKO2_SEL(18);
/* Set clock out1 drives clock out1. */
CCM->CCOSR &= ~CCM_CCOSR_CLK_OUT_SEL_MASK;
/* Disable clock out1. */
CCM->CCOSR &= ~CCM_CCOSR_CLKO1_EN_MASK;
/* Disable clock out2. */
CCM->CCOSR &= ~CCM_CCOSR_CLKO2_EN_MASK;
/* Set SystemCoreClock variable. */
SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
Solved! Go to Solution.
Hi Woodbury
Is SDMMC Stack included in your SDK generated by SDK Dachboard?
fsl_sd.c/h is the source code for UHS-1 SD Card. Init sample code is as follows.
and clock conditions, in my case, It did not work unless USDHC_CLK_ROOT was set to 528 MHz or 594 MHz (this case is still under investigation).
Best Regards,
T.Kashiwagi
Hi Woodbury
Is SDMMC Stack included in your SDK generated by SDK Dachboard?
fsl_sd.c/h is the source code for UHS-1 SD Card. Init sample code is as follows.
and clock conditions, in my case, It did not work unless USDHC_CLK_ROOT was set to 528 MHz or 594 MHz (this case is still under investigation).
Best Regards,
T.Kashiwagi
Takashi,
Thank you for the reply. Your answer worked!
I was using a deprecated pack. I found the MIMXRT1052xxxxB pack, which had the option for the sdmmcstack.
On a side note, it looks like I didn't actually power on the card. I had turned on the pfd and set the usdhc to the correct pfd, but hadn't set the power pin high.