1.Can Co-ordinator use the function to get the Ieee addr of the enddevice???
2.The enddevice's Ieee addr by the co-ordinator calling the ZPS_u64AplZdoLookupIeeeAddr() is zero, when it rejoin a router from the co-ordinator.why?
Hello,
Are you taking into consideration that the required IEEE address will be received in an IEEE_addr_resp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpIeeeAddrRsp?
Also, have you tried retrieving the neighbor table from the coordinator? Also, is the device already in the network?
Regards
Estephania
Hello,
Yeah!Firstly, the enddevice exists in the neighbor table of the coordinator. Secondly, the enddevice rejoin a router.
Hello,
Sorry for the delay, which version of the SDK are you using?
Regards,
Estephania