AnsweredAssumed Answered

DMX512 Slave SDK not working

Question asked by Thiago rodrigues on Oct 16, 2018
Latest reply on Sep 25, 2019 by Kerry Zhou

Hello,

 

I´ve being trying to use the source code and schematic provided by NXP in the AN11153 (DMX/RDM slave) but I can´t seem to make it work.

I´m using a LPC1112/102, and I tried compiling it with LPCXpresso 8 and IAR Worbench 8.32. Both compile with no errors and I flash it using ISP and Flash Magic tool.

 

I seems like either the firmware is not running or simply not working. I don´t know if there is a setting that should be made on the compilers. Just to make sure of it, I added a line in the code turning the LEDs on and OFF, and still does not work.

 

Anyone with experience with this code?

 

Regards,

Outcomes