Hello All,
I need to work on i.MX53 board and it is required to use kernel 3.10.17. Is there any yocto project setup available for this? If not then is there any alternative?
Thank You,
Vatsal
Hello,
Look at the following:
“Building for i.MX Mature Boards”
https://www.nxp.com/docs/en/application-note/AN12024.pdf
Regards,
Yuri.
Hi Vatsal
unfortunately nxp did not release official bsps for that kernel, in mainline kernels
some proprietary drivers like gpu may be absent. One can also look on
Submit i.MX53 & i.MX28 Linux kernel patches
https://community.nxp.com/thread/462874
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igorpadykov
Thanks for quick reply. Can you please specify which latest kernel and BSP we can use for this board?
Can we use 3.0.35?
What is nxp recommendation for the i.mx53 development?
Best Regards,
Vatsal
Hi Vatsal
if you wish to use gpu, recommended to use latest official bsp L2.6.35_11.09.01:
linux-2.6-imx.git - Freescale i.MX Linux Tree
L3.0.35 may lack gpu drivers.
Best regards
igor
latest official bsp was L2.6.35_11.09.01:
linux-2.6-imx.git - Freescale i.MX Linux Tree
I am afraid next, including 3.0.35 may lack gpu drivers.
Best regards
igor