FRWY-LS1012A Serial port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRWY-LS1012A Serial port

1,361 Views
miguel_pineiro_
Contributor I

Hello,

I got a FRWY-LS1012A, and have followed instructions in FRWY-LS1012AGSG.pdf, but I can't get the serial port to show up in the 2 Windows 10 machines I have tried. A disk drive does appear though. What could it be the issue?

On linux I get a /dev/sg2 and /dev/sdc but no "/dev/ttyACM", could this be related?

Thanks

Labels (1)
0 Kudos
3 Replies

1,062 Views
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question concerning the MBED misbehaviour when connected to Windows 10:

https://community.nxp.com/message/1054604?commentID=1054604#comment-1054604 

0 Kudos

1,062 Views
miguel_pineiro_
Contributor I

I did stop the service (it's on the webs getting started instructions) but that did not help. As explained in earlier post, I can't see the serial port device on Linux too.

Should I try the file attached in the other thread? (It's not exactly the same board)

0 Kudos

1,062 Views
ufedor
NXP Employee
NXP Employee

> Should I try the file attached in the other thread?

The FRWY board has K20 MCU - please use attached firmware image.