AnsweredAssumed Answered

imx6ull evk NAND

Question asked by Stefano Cordibella on Oct 11, 2018
Latest reply on Nov 14, 2019 by Ida J

Dear support,

    I am working with a imx6ull evk where we mount a NAND flash Micron 29F4G08ABADA .

I setup the resistor like the volansys gateway that use Micron 29F8G8ABABA and imx6ul.

Now using mfgtool L4.9.11_1.0.0-ga_mfg-tools I have the error that the kernel is unable to erase /dev/mtd0 0 0 .

 

I read that in the mfg tools L4.1.15_2.0.0-ga_mfg-tools it was required a kernel mods and recompile in order to add the GPMI driver in the kernel used to boot the board via usb.

Is it true even with the L4.9.11 that the kernel mod is required?

Do I need to recompile the kernel adding the gpmi driver?

 

Thanks in advance,

Stefano.

Outcomes