Hi,
I have downloaded the zip file named "L4.9.88_2.0.0_images_MX8MQ" from i.MX 8M Evaluation Kit|NXP. I am trying to boot the iMX8M QuadEVK using demo images(). I used linux dd command "$ sudo dd if=<image name>.sdcard of=/dev/sdx bs=1M && sync" (given in the Reference Manual) to flash image to the SD card. I have configured all DIP switches as given in Manual. (With the same configuration I am able to boot Android from SD card).
Am I missing any steps to follows ?
Kindly help me to bringup the board
Thanks,
Girija Pretha
Hi Girija
one can try with other sd card or using mfg tool, use script
mfgtool2-yocto-mx8-evk-sd2.vbs.
"Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX8MQ BSP"
Demo Images
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------