Starting local server...
Successfully started gdb server 127.0.0.1:45002.
Set gdb remote timeout to 7200
Connecting to target...
Using LS1012A SoC
Using CMSIS-DAP
Using jtag speed 6000
Connecting to probe...
ccs:USB not configured
connected successfully
Successfully connected to probe
Initializing target...
Running init script c:\freescale\cw4net_v2018.01\cw_armv8\armv8\gdb_extensions\flash\scripts/../../../../Config/boards/LS1012A_FRDM_init.py
ccs:There is no chain configured - chain size is zero
Target reset failed.
Can you tell me the cause of the error?
I attached cwflash.py to the body.
1) Is the board capable to boot?
if not:
2) Is valid RCW present in flash?
> Resistance to R50, is this a hard coded RCW?
Yes, this is hard-coded RCW option.
The board can't boot with hard-coded RCW - refer to the QorIQ LS1012A Reference Manual, 4.4.5.2 Hard-coded RCW options.
The hard-coded option normally should be used to program a valid RCW into the flash.
I made a mistake.
It works well after connecting to JTAG for CMSISDAP.
Thank you for your help.
Please provide the modified "cwflash.py" for inspection.