Hi!
I am using T2080 board and interfacing NOR Flash to IFC.
i am confused in IFC Flash Timing Registers. I have read the reference manual but i can not decide that what values should i set in all timing registers and what is the value of ip clk and IFC module input clocks that is used in reference manual.
Thank you
Regards,
Anshul Khare
> what values should i set in all timing registers
Please refer to the attached CodeWarrior initialization script for the T2080RDB - it contains IFC registers initialization.
> what is the value of ip clk and IFC module
For the IFC ip_clk (IFC module input clock) refer to the T2080 Reference manual, Figure 4-3. T2080 Logic Clock Subsystem Block Diagram - 1/2 Platform clk.
For the IFC clock (IFC_CLK) frequency refer to the T2080 Reference manual, 13.3.32 Clock Control register (IFC_CCR), CLKDIV
Hello ufedor
Thanks for reply.
CodeWarrior initialization script for the T2080RDB is not attached in your reply.
please provide the same.
Regards,
Anshul Khare
Definitely it is attached - please see the screenshot:
yes got it.
Thanks :smileyhappy: