I am using IMX7dea Ucom Som board and Ksz8895 ethernet switch chip.I used SPI interface between mpu and ethernet chip.I add linux driver to mey kernel but i didnt see xx.o file.I guss ccross compile didnt worked.Ant it didnt creat xx.o files.I used KSZ8895 Linux driver for revision 3.3 tared.
How can I fix this?
Also I saw writing blove these in KSZ8895MQ/RQ Evaluation Board User’s Guide
The KSZ8895 will power up initial default configuration with the start switch in register 1 bit 0
= ‘0’ which means the switch is “off”. You can set the bit 0 =’1’ to start switch.
How Can I change this register with spi interface?
Thanks.
Hi Emin
one can look at Yocto project documentation
Adding the WF111 Driver to the i.MX6 Yocto BSP
https://community.nxp.com/thread/444387
i.MX Yocto Project: How can I (quickly) modify the kernel and test it?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------