AnsweredAssumed Answered

Load Switch ILim Pin issue

Question asked by kiran Habib on Oct 7, 2018
Latest reply on Oct 9, 2018 by G.w. Sun

Hi,

 

We are using the NX5P3290UKZ load switch in our design.
The input to the switch is 5V at 3A(max) and output is limited to 5V at 1A using resistor of 49.9Kohm on ILim pin of switch.
We are seeing an issue that when we power ON the board the ILim pin of switch get shorted with ground(0ohm with respect to ground).
Kindly let us know your thoughts on the same.

 

 

Thanks & Regards,

Kiran

Outcomes