AnsweredAssumed Answered

Empty output when using custom linker script

Question asked by Diego Barile on Oct 5, 2018
Latest reply on Oct 5, 2018 by Con Verse

Hi guys.

 

I'm developing the FW of one LPC11C24 board using LPCXpresso v8.0.0 [Build 526].
When I trying to using a custom linker script to shift the release code from sector 0 to sector 1 (0x1000) the compiler generates one empty output like the follow:

 

ext databssdec hex filename
00000LeMiG.axf


The output file LeMiG.axf is empty.
If I keep the default script all builds fine.


I've attached my custom linker file.


Where I wrong?
Thanks in advance.

 

Diego.

Attachments

Outcomes