AnsweredAssumed Answered

1920 x 720 HDMI monitor porting

Question asked by HUN KIM on Oct 4, 2018
Latest reply on May 26, 2019 by kokshyangchin

Hello, since our imx6qdlsabreauto board doesn't interact with 1920x720 custom monitor (LA123WF4)

 

Here is what I have been done so far

 

1) With devshell command, I have modified mxc_hdmi.c / mxc_edid.c / mxc_edid_h / imx6qdl-sabreauto.dtsi in kernel-source

 

in mxc_hdmi.c

    static const struct fb_videomode vga_mode = {
            /* 1920x720 @ 60 Hz, 31.5 kHz hsync */
            NULL, 60, 1920, 720, 11112, 56, 56, 4, 4, 16, 2,
            FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_8_3, 0
    };

 

in mxc_edid.c

    /* #48: 1920x720p@60 16:9 */
     [48] = {
        NULL, 60, 1920, 720, 11112, 56, 56, 4, 4, 16, 2,
        FB_VMODE_NONINTERLACED | FB_VMODE_ASPECT_8_3, 0
     },

 

in mxc_edid.h

    #define FB_VMODE_ASPECT_8_3      0x40
    #define FB_VMODE_ASPECT_MASK    (FB_VMODE_ASPECT_4_3 | FB_VMODE_ASPECT_16_9 | FB_VMODE_ASPECT_8_3)

 

in imx6qdl-sabreauto.dtsi

mxcfb1: fb@0 {
                compatible = "fsl,mxc_sdc_fb";
                disp_dev = "hdmi";
                interface_pix_fmt = "RGB24";
                mode_str ="1920x720M@60";
                default_bpp = <32>;
                int_clk = <0>;
                late_init = <0>;
                status = "okay";
};

 


2) Compiling all the changes, and building all images including zImage and dts with yocto with below commands

 

bitbake -C compile virtual/kernel

bitbake fsl-image-multimedia-full

 

 

 

3) in uboot, I have changed

setenv panel Hannstar-XGA

 

setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=PARTUUID=${uuid} rootwait rw video=mxcfb0:dev=hdmi,1920x720M@60,if=RGB24'

 

setenv video_args_hdmi 'setenv video_args $video_args video=mxcfb${fb}:dev=hdmi,1920x720M@60,if=RGB24'

 

But still, it does not work well, the display only gives white screen. And fbset value is like below.

 

root@imx6qdlsabreauto:~# fbset

mode "1920x720-60"
    # D: 89.993 MHz, H: 43.942 kHz, V: 60.194 Hz
    geometry 1920 720 1920 720 32
    timings 11112 56 56 4 4 16 2
    rgba 8/16,8/8,8/0,8/24
endmode

 

 

I suspect several possible reasons.


1) Might hdmi_timing is wrong calculated. If it is, I was wondering if you could check it out with https://www.lcdtek.co.uk/img/cms/PDF/LA123WF4-SL01_2017.pdf detail information

 


2) Might use HDMI_ASPECT_64_27 not FB_VMODE_ASPECT_8_3, **because I already confirmed that the display works well with the raspberry pie 3 board and below command in config.txt**
hdmi_timings=1920 0 0 2 126 720 0 2 2 4 0 0 0 60 0 89456640 8
The last 8 option means HDMI_ASPECT_64_27. So if it is, how can I need to change in mxc_edid.h

 

    #define FB_VMODE_ASPECT_64_27      ????

 

3) Based on the display T-Con board specifications, its input is DVI input using HDMI cable (TMDS), it might be a problem?

 

Thanks in advance!

Outcomes