AnsweredAssumed Answered

QN9080 BLE Without OS Abstraction

Question asked by CICERO DOMINGOS JUNIOR on Oct 3, 2018
Latest reply on Oct 4, 2018 by George-lucian Capraru

Hello friends,

 

I'm developing an application based on QN9080. This application should read values from two I2C sensors and store in a buffer in a Flash SPI memory. At 15-second intervals it should send the stored data, arranged in formatted packets, via BLE to a Smartphone application.  So, I'd like to write the QN9080 software in the simplest way possible. I already have the base application running with FreeRTOS, performing the readings of the sensors, writing on an OLED display and storing in flash memory. I need to implement BLE communication without using the OSAbstraction layer. Can anybody help me ?

Outcomes