AnsweredAssumed Answered

running startx from the console disables the console

Question asked by David Luberger on Oct 2, 2018

For whatever reason, startx isn't running automatically when my device starts up.  If I enter the startx command from the console, the lxde desktop comes up fine.  However, since I ran startx from the serial port console, the console itself is now longer accepting command inputs because the startx command is actively running. I can type but it's no longer at a shell prompt, and typing anything doesn't cause a response from the shell. If I hit ctrl-c it kills the desktop that was running on the lcd screen but I then get back to the shell prompt.  Is there a way to load the desktop without it "consuming" my serial terminal?  I've read about getty, but I can't do things like switch terminal sessions with ctrl-alt-f2 etc. because I can't send ctrl-alt commands through my serial window (unless that's just a matter of changing settings).

Outcomes