Hello
Im'working on imx6Q cpu with SSI audio interface. SSI1 works very well into playback and capture mode.
The problem is:
I would like to improve it. I notice that if have a fault on physical bitclock signal I have a problem. In particular in Network mode (with more then 1 slots) slot shift of 1 slot respect the frame sync. the same problem there isn't if I have a fault on frame sync signal.
I enable interrupts on SIER and I see into SISR RFS, TFS, RLS and TLS flags.
I would like to see 1 flag of RFS and after 1 flag og RLS. Flags showed randomic events.
I hope someone help me.
thanks
Marco from Italy
Hi Marco
once initialized, special sequence may be required for changing SSI parameters,
it is better described in older SSI documentation like
sect.56.5 Initialization/Application Information i.MX51 Reference Manual
https://www.nxp.com/docs/en/reference-manual/MCIMX51RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadykov,
I will check the sequence.
thanks
Marco