Building u-boot for imx8mm_evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building u-boot for imx8mm_evk

1,388 Views
mahmed
Contributor I

Hi,

I'm trying to build and bring up U-boot for imx8mm_evk board. It looks like imx8 requires bunch of files to build the bootloader. The file that will eventually be put onto SD card is called 'imx-boot' genereated by imx_mkimage tool in combination of following four files: SPL, U-boot, ARM Trusted Firmware, DDR firmware.
My question is where do I get DDR firmware from. One of the README files say following but I can't access the repository:

1. DDR PHY firmware images (Mandatory, used for all targets)
Files: lpddr4_pmu_train_imem.bin and lpddr4_pmu_train_dmem.bin
Git: ssh://git@sw-stash.freescale.net/imx/linux-firmware-imx.git
Directory: firmware/ddr/synopsys

Any help is appreciated.

0 Kudos
1 Reply

787 Views
diegoadrian
NXP Employee
NXP Employee

Hello

Unfortunately, we still do not have support for the i.MX8MM since the product is still in preproduction and we do not have a way to test the problem. I apologize for the inconveniences.

Best regards,

Diego.

0 Kudos