In My_Wireless_App there are two files called "MC9S0...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In My_Wireless_App there are two files called "MC9S0...

672 Views
Juan
Contributor I
In My_Wireless_App there are two files called "MC9S08gt60.c" and "MC9S08gt60.h." In this file are given the registers of status, control and configuration of the AD converter. To access these registers do, for example
# include "MC9S08gt60.h."

However, I can not have access to the values of those registers.

In "MC9S08gt60.h" they are defined as follows:

typedef union {
    Byte Byte;
    struct {
       "registers"
    }Bits;
  } AT1SC;

How do I configure these registers?
Labels (1)
0 Kudos
1 Reply

178 Views
Ake
Contributor II
Hi,
Use
#include "derivative.h"
instead.
then the compiler will pick up the correct .h file for you. That is the MCU that is in "Change MCU/Connection...."
 
Regards,
Ake
0 Kudos