Kernel Crash in Yocto BSP L4.9.88_2.0.0-ga

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel Crash in Yocto BSP L4.9.88_2.0.0-ga

714 Views
sagar_sakre
Contributor I

I am following i.MX Yocto Project User's Guide from https://www.nxp.com/docs/en/user-guide/i.MX_Yocto_Project_User%27s_Guide_Linux.pdf 

I was able to build it and flash it successfully but while booting I am getting kernel crash.

Can anybody please let me know what could be the issue?

I using IMX 7 sabre dual board. I've attached the complete log.

Kernel BUG at 8009fdac [verbose debug info unavailable]  Internal error: Oops - BUG: 0 [#1] PREEMPT SMP ARM  Modules linked in:  CPU: 0 PID: 1 Comm: ���per/0 Not tainted 4.1.44-fslc+g6c1ad�� C  r : [<80942160>]    psr: a00001d3  0+0x60/0x84)���hU�����[<80942160>] (__do_kernel_fault.part.0) from [<8001f888>] (do_page_fault+0x38c/0x3a0)��`Oł[<8001f888>] (do_page_fault) from [<8001f9dc>] (do_tr� Booting Linux on physical CPU 0x0  Linux version 4.1.44-fslc+g6c1ad49 (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #1 SMP PREEMPT Fri Sep 21 12:24:20 IST 2018  CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d  CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache  Machine model: Freescale i.MX7D SabreSD Board  Reserved memory: created CMA memory pool at 0xac000000, size 320 MiB  Reserved memory: initialized node linux,cma, compatible id shared-dma-pool  Memory policy: Data cache writealloc  PERCPU: Embedded 13 pages/cpu @ab71a000 s21068 r8192 d23988 u53248  Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096
Labels (1)
Tags (2)
0 Kudos
1 Reply

496 Views
igorpadykov
NXP Employee
NXP Employee

Hi sagar

one can try to rebuild image from scratch and use for programming image mfg tool from

i.MX Software|NXP 

Please use mfg tool version corresponding to used linux kernel version.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos