Imx6 port uboot and display logo in uboot stage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 port uboot and display logo in uboot stage

Jump to solution
594 Views
864535720
Contributor II

hello,Dear community,  I want to display the logo through LVDS when uboot starts. The uboot version I used is 2015-04, and my chip is IMX6D. I have not made any changes to uboot, I can specify through the debug information, uboot executed enable_lvds(), and also executed video_init, video_logo and other functions, but my screen did not respond at all, then when I went to measure, I Found that lvds has no signal. Because in the kernel phase, my screen is displayed properly, so I think my hardware is no problem. Maybe it's a problem with my uboot configuration. Can you help me see where I need to change?

Labels (1)
0 Kudos
1 Solution
389 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东 刘

please try patches on

https://community.nxp.com/docs/DOC-98109 


Best regards
igor
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
390 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东 刘

please try patches on

https://community.nxp.com/docs/DOC-98109 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos