How to flash Images to eMMC using MfgTool2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to flash Images to eMMC using MfgTool2?

970 Views
byunggukchoi
Contributor II

I'm trying to flash bootloader, kernel and rootfs into eMMC on IMX8MQ EVK with MFGTool2.

When running mfgtool2-yocto-mx8-evk-emmc1.vbs after downloading 4.9.88_2.0.0_mfg-tool_MX8MQ.tar.gz from NXP website, MFGTool2 returns the following error.

"Boot" body="BootStrap" error, file="C:\mfgtools\Profiles\linux\OS Firmware\firmware\imx-boot-imx8mqevk-sd.bin-flash_evk""

The settings of cfg.ini is default as described in "i.MX_Linux_User's_Guide.pdf".

The document says the default settings is for i.MX6 SoloX.

Then how to change the settings to flash eMMC on IMX8MQ EVK?

And I find that there is a directory named as "mfgtools\Profiles\Linux\OS Firmware\files\android".

But "linux" directory does not exist. I have built the yocto source code for linux version.

What should I modify to flash linux images into eMMC?

And any other information to flash images into eMMC using MfgTool2 will be helpful.

Thanks in advance.

0 Kudos
1 Reply

460 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 Look at the following:

mfgtool imx8mq evk fails 

  Also, please check if  USB-UART driver of Silicon Labs is installed on the host PC.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos