Dear NXP:
Camera output YUV 8-bit stream, what should i do with S32DS ISP Graph Tool?
and which IPUS kernel should i select to handle it ? like below capture shows, is there more documentation about the kernels?
Please help to support, thanks a lot.
My debugging enviroment:
Hardware: S32V234EVB (Mainboard) + MAX9286S32V234DB (Deserializer) + LI-OV10640-490-GMSL-055H(Camera, attached datasheet)
Software: isp-ov10635-quad (VSDK Demo)
Running the demo 'isp-ov10635-quad', get error:
Failed to grab image number 0