CLRC663+ : leakage current in standby mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663+ : leakage current in standby mode

642 Views
oliviergiard
Contributor I

Hello,

I have a board with CLRCL663+ drived by an STM32L4.

CLRCL has VDD=3.3v (same voltage for STM32) and TVDD=5V
When I apply 1 to the POWERDN pin of the CLRC the power consumption is nearly 24uA
When the the POWERDN pin is 0 and I set the standby bit (bit 7, register 00h) to 1, the IC goes in standby mode but the power consumption is nearly 400/500uA instead of the 8uA in the datasheet.

Does anyone has this problem too?

Thanks

Regards

Olivier

Labels (2)
Tags (3)
0 Kudos
0 Replies