When using MCUXpress simulation code that work on LPC54608 - writen with ”complex.h” with support from Newlibnano its working.
If Redlib is used it dosent work.
What is the "right/corect" C-lib variants that should be used moving forward?
Redlib, Newlibnano, NewLib?
Thanks,
Jakob Riis
Hello Jakob Riis,
• Redlib Our own (non-GNU) ISO C90 standard C library, with some C99 extensions.
Can't used to C++ project.
• Newlib GNU C/C++ library
• NewlibNano a version of the GNU C/C++ library optimized for embedded.
About the difference among these libraries, you can have a look at:
How to Switch C/C++ Library in MCUXpresso IDE
or the detail information in <MCUXpresso_IDE_User_Guide>->
15. C/C++ Library Support
Hope it helps,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------