Technical Inquiry on BGU6102

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technical Inquiry on BGU6102

427 Views
jenita
Contributor I

Hai

I would like to know about the LNA parameters specifications(Gain,NF,IIP3 etc) when the amplifier is disabledAnd is it applicable for TETRA Handheld Radios?

Tags (1)
0 Kudos
1 Reply

360 Views
LPP
NXP Employee
NXP Employee

You can find some of the power-down parameters in this application note:
https://www.nxp.com/docs/en/application-note/AN11866.pdf

This device can be used as LNA for TETRA application. Please note that the ENABLE is provided to implement power-down feature. It is not suited for fast signal modulation.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos