Hi Hi
I am using T2080RDB-PC to research.
I have a question about T2080RDB-PC's security.
Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?
Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??
THANK U
> Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?
When Secure Boot is enabled the "cold boot" attack is impossible - refer to the:
https://www.nxp.com/docs/en/brochure/PWRARBYNDBITSTA.pdf
https://elearning.nxp.com/enrol/index.php?id=254
> Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??
USB ports of the T2080RDB are equipped with VBUS054B-HSF ESD protectors.