ETHERNET fm1-mac3 is not visible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETHERNET fm1-mac3 is not visible

786 Views
anshulkhare
Contributor III

Hello All,

i have T2080RDB board when i am loading kernel image .dtb and root file system i am not able to see

fm1-mac3 in logs.

i am able to see only fm1-mac9 and lo.

i am generating binary using fsl image core.

how to solve this.

Regards

Anshul

0 Kudos
2 Replies

643 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anshul khare,

Probably you use shared-mac dtb file, all Ethernet interfaces are assigned to USDPAA and fm1-mac9 is defined as shared-mac interface, so you only can see it in Linux.

Please use normal dtb file naming without usdpaa.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

643 Views
anshulkhare
Contributor III

Hello yipingwang

Thank you for support !!

problem is solved, i was using wrong dtb File.

Regards,

Anshul

0 Kudos