AnsweredAssumed Answered

Developing in S32 Design studio for Vision for the SBC-S32V234

Question asked by Kaartic Sivaraam Sankaranarayan on Sep 26, 2018
Latest reply on Oct 9, 2018 by Kaartic Sivaraam Sankaranarayan

Hi,

 

We are evaluating the SBC-S32V234 development board in our company. I have flashed it with the pre-built BSP v18.0 that comes with the Vision SDK 1.2.0 release. I would like to develop some ISP and APEX programs using the S32 Design Studio for Vision v2.0.

 

I initially tried to build a demo application. The build succeeded but I found that the demo application binary built using the S32 Design studio v2.0 doesn't work as it is on the SBC-S32V234 which has been flashed with the BSP v18.0 + Vision SDK v1.2.0. I suspect it's possibly due to the fact that the S32 Design studio uses the Vision SDK v1.0.0 to build the binaries.

 

How am I supposed to develop ISP and APEX application in the S32 Design Studio v2.0 for the SBC-S32V234? Should I change the BSP? If yes, what version? I could not find any information about the latest version of BSP that is compatible with both the Vision v1.0.0 and the SBC-S32V234.

 

Any related information/pointers would be helpful.

 

Thanks,

Sivaraam

Outcomes