Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

Jump to solution
715 Views
harrytan
Contributor I

Hi, I understand that currently i.MX8M BSP is only supported in Linux kernel 4.9.x. Do NXP has plan to support i.MX8M in Linux Kernel 4.14.x?

Labels (2)
Tags (2)
0 Kudos
1 Solution
558 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
3 Replies
559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harry

yes there are plans to support i.MX8M in Linux Kernel 4.14.x.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
558 Views
harrytan
Contributor I

Hi Igor,

Do you know when is estimated release date for the BSP?

Regards,

Harry

0 Kudos
558 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harry

seems by the end of year.

Best regards
igor

0 Kudos