AnsweredAssumed Answered

MPC5777C and STCU2_LB_PCSn limits

Question asked by Maurizio Greco on Sep 24, 2018
Latest reply on Mar 1, 2019 by Peter Vlna

Hi, 

I'm searching information about value to be used for STCU2_LB_PCSn limits.

I found in the AN5288.pdf value for 90% of coverage. But I have not understand how values of that register can be modified in order to achive a different value of coverage.

 

Can I suppose linear relation must be used?

 

In other words: for example, in the application notes AN5288 is reported for STCU2_LB_PCS2 (3N45H) 0x500 for 90%, can I suppose value for 100% is equal 0x58E?  Is really so simple? Or we need to have another kind of details to modify % of coverage?

 

Thanks in advance for answer.

Outcomes