The compile is looking for the portasm_JN516x.s file in ../../ExtendedColorLight/Build/ while it is located in the sdk/JN-SW-4170/Components/ZigbeeCommon/Source
I've had this problem with the JN-SW-4168 also compiling other projects, but never managed to fix it.
Thank you,
Hi Charles,
Be sure that you are set as active the example that you are working on.
Regards,
Mario
Hello Mario,
Yes I do have the LIGHT attribute set properly.
The file portasm_JN516x.S does exist in JN-SW-4170/Components/ZigbeeCommon/Source but it seems the Makefile does not find it or does not look for it.
I've installed Beyond Studio, the JN-SW-4170 SDK and the JN-AN-1218 as required in the default locations...
Thank you,
Found it:
It has something to do with the SDK_BASE_DIR that was not setup correctly, I changed it to the line below. I've also added the COMPONENTS_BASE_DIR definition as it didn't seem to exist.