BOOTCFG pin active high or low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BOOTCFG pin active high or low

Jump to solution
710 Views
wilco_work
Contributor I

Hello all,

I'm using the K82FN256 and want to use the BOOTCFG0 pin for booting. Is this BOOTCFG0 active HIGH or active LOW (asserted by logic 1 or 0)?

Kin regards

Tags (2)
1 Solution
594 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

View solution in original post

0 Kudos
2 Replies
595 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Jan,

Based on the following table of the reference manual. 

pastedImage_1.png

We can know that the pin is active high, asserted by logic 1. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
594 Views
wilco_work
Contributor I

Hi Victor,

Thank you! Apparently putting a high value at the pin will result in a 1 at the register. I missed that point.

Kind regards