Hello S12Z team,
I am trying to flash and this message comes up..
"Can't program 8 bytes to address 0xff0128 because this range isn't included in the selected modules! "
Flash Operation. ...
Auto-detection is successful.
File is of type Motorola S-Record Format.
Device MC9S12ZVMC128_EEPROM
Programming ....
Programming warning. Can't program 8 bytes to address 0xff0128 because this range isn't included in the selected modules!
Programming .......
Programming warning. Can't program 8 bytes to address 0xfffdf8 because this range isn't included in the selected modules!
Programming ........
Device MC9S12ZVMC128_EEPROM
Program Command Succeeded
Flash Operation. done
What I am doing wrong? What I have to change that this doesn't shows up.
Thank you
Hello,
I only want to program Flash.
I just created a new project in codewarrior and used Flash file to target and there I used my own ".S2" file.
Hello,
So you use the S12Z Flash Programmer Task and select Flash device, right?
Regards,
Daniel
Hi,
The two addresses are not EEPROM but flash.
What do you want to program? EEPROM or Flash?
How did you configured the Flash Programmer?
Regards,
Daniel