How to config CAN RXFIFO on MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to config CAN RXFIFO on MPC5748G

1,453 Views
yukunwu
Contributor III

Hi, All,

       I'm using MPC5748G devkit to implement CAN Receice an CAN Send. 

       I saw there is an example code in "S32_SDK_MPC574xx_EAR_0.8.1" about FLEXCAN but it is only show how to receive an static CAN ID's message by using API[ FLEXCAN_DRV_Receive(uint8_t instance,uint8_t mb_idx,flexcan_msgbuff_t *data)]. I want to receive many CANID's message and then to sort and handle them, but i don't know how to config. 

       Could you please provide an example for me? Thanks~

uint32_t fifo_filter[5] = {0x111,0x222,0x333,0x444,0x555};
flexcan_id_table_t config_fifo = {
.isRemoteFrame = false,
.isExtendedFrame = false,
.idFilter = fifo_filter,
};

FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);

FLEXCAN_DRV_SetRxMaskType(INST_CANCOM1, FLEXCAN_RX_MASK_GLOBAL);

FLEXCAN_DRV_SetRxFifoGlobalMask(INST_CANCOM1, FLEXCAN_MSG_ID_STD, 0x1FFFFFFF);

FLEXCAN_DRV_ConfigRxFifo(INST_CANCOM1, FLEXCAN_RX_FIFO_ID_FORMAT_A, &config_fifo);


flexcan_msgbuff_t recbuff;
for (;;) {
FLEXCAN_DRV_RxFifo(INST_CANCOM1, &recbuff);
}

Labels (1)
0 Kudos
2 Replies

866 Views
alexandrunan
NXP Employee
NXP Employee

Hello Wu,

You can find an example of initialization and read of CAN Rx FIFO here https://community.nxp.com/thread/473207  .

I advise you to use latest version of SDK available for Power Architecture RTM 2.0

BR,

Alexandru Nan 

0 Kudos

866 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately we do not have the example you are asking for, however you maybe fond use for examples which need to be ported tho MPC5748G micro from our repository:

Example MPC5744P FlexCAN TX RXFIFO ISR GHS614 

https://community.nxp.com/docs/DOC-329623 

regards,

Peter

0 Kudos