AnsweredAssumed Answered

Error in simulation with NXP LDMOS device model in Keysight ADS

Question asked by Sanjeev Ghildiyal on Sep 18, 2018
Latest reply on Sep 25, 2018 by Sanjeev Ghildiyal

Error in simulation with NXP LDMOS device model in Keysight ADS

 

Model Kits installed: 

  • RF_Power_ADS_DesignKit_ads2017p1p9
  • AFT27S010N_Level2_Rev0_DK

Keysight ADS version: 2015.01

 

Error Message while doing DC simulaiton: 

(stdcmds.ael line 261, column 30)

Error generating netlist for "NXP_LDMOS_modelTest_01_lib:cell_1:schematic": Failed to create netlist:

In design `NXP_LDMOS_modelTest_01_lib:cell_1:schematic':

The instance `I__0' has 4 pins, but the view `AFT27S010N_Level2_Rev0_DK:FSL_AFT27S010N_Level2_Rev0_MODEL_FET2:layout' has 0 pins.

(stdcmds.ael line 261, column 30)

Error generating netlist for "NXP_LDMOS_modelTest_01_lib:cell_1:schematic": Failed to create netlist:

In design `NXP_LDMOS_modelTest_01_lib:cell_1:schematic':

The instance `I__0' has 4 pins, but the view `AFT27S010N_Level2_Rev0_DK:FSL_AFT27S010N_Level2_Rev0_MODEL_FET2:layout' has 0 pins.

 

Please help in resolving the issue.

 

Attached ADS project for reference, and snapshot of error report.

 

Thanks 

Outcomes