AnsweredAssumed Answered

The debugger can not connect to the P&E device

Question asked by Ivan P on Sep 18, 2018
Latest reply on Sep 25, 2018 by xiangjun.rong

Hi,

 

I am using MC56F82748VLH MCU and I recently installed the CodeWarrior v11.0 on my Windows 10. I also installed the P&E driver for the Multilink Universal.

 

Unfortunately, after building the project the debugging process can not be completed. I believe that the specs of my laptop are much higher than the minimum requirements (8GB RAM and i5 7th Gen processor) so I believe the problem is not in the computer. The errors I get are as follows (can also be seen in the attached files):

 

"Error launching MC56F827...._SDM_Universal_Multilink. GDI Protocol fatal error: Unknown Fault. The debugger can not connect to the P&E device."

 

"An error occurred while connecting to the interface hardware or target specified in the Launch Configuration Dialog. For this launch, you may retry/re-specify the connection with the following parameters:

-UMultilink Universal Rev C

-OSJTAG"

 

Do you know how can I resolve this issue and is the Windows 10 compatible with CW11 an P&E software?

 

Thank you.

Outcomes