AnsweredAssumed Answered

Can FEC memory be used as general-purpose RAM?

Question asked by Etienne Alepins on Sep 14, 2018
Latest reply on Sep 24, 2018 by David Tosenovjan

In the MPC5777C, I will not be using the FEC Ethernet controller. However, it would be nice if I could increase the total internal RAM such that the cores/applications could put variables in the FEC internal RAMs. Is that possible?

 

Also, what is the size and number of RAMs embedded in the FEC?

 

Thanks.

Outcomes