I'm using i.mx6q sabresd board, and the Linux kernel is downloaded from here: GitHub - MrVan/linux: Linux kernel source tree .
The problem is that the linux network socket seems don't work. When I write an application to create a socket, it is blocked. The network is ok, as the ping works well.
Following is the code I want to create a socket. However, it is blocked, and doesn't run.
//Create socket
sock = socket(AF_INET, SOCK_STREAM, 0);
if (sock < 0){
printf("Could not create socket");
exit(0);
}
Hi shijun
according to attached Release Notes sect.2.1 New features nxp linux sources are located on
Supported functionality and drivers are described in attached Release Notes sect.3 BSP Supported Features
and Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------