AnsweredAssumed Answered

pcie loopback

Question asked by viniamin tokarchuk on Sep 12, 2018
Latest reply on Sep 17, 2018 by Yiping Wang

Is there anyway to configure a QorIQ processor such as the T2081 to do loop back of the TX signals onto the RX signals? I have an FPGA on one endpoint that can run PCIe tests but only if the other end is looping back the signals. On the FPGA it is called serial loopback mode, anything similar on the CPU side? 

 

Thanks,

Vinny

Outcomes