AnsweredAssumed Answered

LPC2478 LCD clock

Question asked by SIVA BOMMARAJU on Sep 12, 2018
Latest reply on Sep 14, 2018 by CarlosCasillas

HI,

I have configured the LPC2478 LCDDCLK clock to 24MHz O/P and observed that the clock is not reaching to full 0VDC on the negative transition.

I have made the following measurements and observe the issue:

1) Configured the DCLK at Pin 150 to 14MHz and observed the sine wave clk  with slow rise and fall times.

2) When it is configured to 24MHz clock the clock signal is not  reaching to complete 0VDC on the negative transition.

 

Can you please suggest the root cause and possible trouble shooting techniques on this.Measurement WF are attached for reference.

 

Thanks ,

 

Siva Bommaraju

Attachments

Outcomes