AnsweredAssumed Answered

What is the minimum supply voltage to S12ZVL?

Question asked by 展辉 刘 on Sep 12, 2018
Latest reply on Sep 12, 2018 by Daniel Martynek

Dear NXP Enginner,

           I have a quetion about work voltage with S12ZVL ,check with datasheet ,it shows normal operation voltage is 5.5~18v.What does the“  Operation down to 3.5V is guaranteed without reset, however some electrical parameters are specified only in the range above 4.5 V ”  means ? 

          If the input voltage is from 4.5V to 5.5V ,if MCU can work normal ?  And how about the MCU status in 3.5v~4.5v ? 

Outcomes